Location: Milton, NY
Your internet browser isn't supported.
Venue
The Hudson Valley Sports Dome is an air-supported indoor sports dome located in Milton, NY. Nearly any sport played on a turf field is played in the dome, which is among the largest in the Northeast, including soccer, field hockey, lacrosse, softball and flag football. It has also hosted everything from home and garden shows to dog shows, wrestling tournaments, graduations and corporate events.
Challenge
Operators wanted more light and more natural light, and had been looking for alternatives to their legacy metal halide lighting for a long time. Given the size of the dome, it was very difficult to get adequate lighting to ensure the safety of athletes while playing. Energy and maintenance costs were high, and the operators were looking for “green” upgrades they could make throughout the facility.
Scope
The project included replacing all of the metal halide lights in the dome. With the dramatically reduced fixture count, just two Ephesus fixtures were mounted on each crossarm, replacing six metal halides installed previously.
Solution
32 Ephesus LED fixtures were installed around the dome’s perimeter, replacing 96 1000W metal halide fixtures. This installation is unique in that the fixtures were installed to cast light upward onto the reflective surface and ceiling of the dome to direct the light back down to the playing surface. This was the first use of the Ephesus Stadium series fixtures in this mounting configuration and the first known use of LED lighting in an indoor sports dome.
Results
Estimated energy consumption was reduced by 75% and an average of 45 foot candles was generated on the playing surface, far exceeding the original lighting’s measurements of 15 foot candles. The indoor lighting more closely replicates natural daylight, an important attribute in a facility with no windows. The Ephesus fixtures eliminated shadows and dark spots on the playing surface for an improved experience for both players and spectators.
Inferior lighting has been an issue in our facility for a long time. We have waited for this lighting technology for over ten years. What Ephesus has brought to our dome in terms of energy efficiency, improved safety and lighting quality has definitely exceeded our expectations.Nick Pizza, owner/operator, Hudson Valley Sports Dome