Open-standard DALI-2 control. Auto-addressing.
App-based commissioning. No specialist required.
Your internet browser isn't supported.
DALI-2 Certified
Open-standard. Cross-manufacturer Interoperability. Already written into most commercial spaces.
Same-day Commissioning
Auto-addressing get system online fast. Most crews finish the day they install. No specialist needed.
No Specialist Required
Your electricians. The WaveLinx app. Precise diagnostics when you need them. No callbacks.
WHY WAVELINX DALI
Built to Simplify Every Part of the Workflow. Spec Through Commissioning.
Installation-Friendly Wiring
Control wiring can be installed without dedicated conduit. It can share conduit with line voltage. That simplifies rough-in, reduces material and labor cost, and keeps the project schedule moving.
Ceiling Topography
Adjust zoning, scenes, and fixture behavior in WaveLinx software. Not by pulling cable. Not by opening ceilings. If a zone needs to be reconfigured, it is a software change. That is it.
Instant Digital Diagnostics
Digital addressing means digital diagnostics. When something is off, WaveLinx DALI tells you exactly what and where. No trial and error. No physical inspection of every fixture. Fewer callbacks.
HEALTHCARE + CRITICAL ENVIRONMENTS
Complex Specs. Handled.
Complex healthcare specs require control that maps precisely to zone types. Patient rooms, corridors, procedure suites. Each has its own requirements, and commissioning has to happen in narrow after-hours windows without disrupting care.
WaveLinx DALI commissions zone by zone, on your schedule, through the app. Submittal documentation is generated automatically. DALI-2 interoperability means the spec already fits.
ELECTRICAL CONTRACTORS
Finally, It Just Works.
Legacy DALI commissioning required a specialist, a laptop, and an afternoon no one was getting back. WaveLinx DALI replaces that entirely. Your electricians open the app. The system auto-discovers and addresses every fixture. Commissioning is done before they leave the site.
If a fixture is swapped post-install, the app re-addresses it in minutes. No re-commissioning the zone. No callback. No second trip.
CLEARING THE RECORD
DALI has a reputation problem. Most of it is not true.
These are the four objections that live in every specifier’s head before the first email is opened.
Here is what the facts actually say
Four more myths. Eight truths. All documented and ready to share with your client or your team.
HOW IT STACKS UP
WaveLinx DALI vs. Common Control Alternatives
MOST DALI PROJECTS FAIL FOR THE SAME REASONS
The Guide That Covers All of Them.
Most DALI projects run into the same commissioning pitfalls. Most are preventable at the spec stage, before a vendor is selected and before a bid goes out.
Commissioning pitfalls. Vendor comparisons. The five questions every vendor has to answer. No commitment.
I’M SPECIFYING THE PROJECT
Everything You Need to Lock the Spec.
Spec sheets, brochures, and submittal documentation. WaveLinx DALI is DALI-2 certified, cross-manufacturer compatible, and built for projects that cannot afford an interoperability problem at commissioning.
I’M INSTALLING THE PROJECT
Your Crew’s On-Site Workflow.
Twenty minutes. We walk through the commissioning workflow for your project type. What the app does. What the crew does. How long it takes. No commitment.
SYSTEM ARCHITECTURE
Open Standard. Hybrid-Ready. Already in the Spec.
WaveLinx DALI runs on the DALI-2 open standard. It is interoperable with other DALI-2 certified devices and already written into most commercial specs by name. The standard is governed by the IEC and a global consortium.
There is no vendor lock-in. It integrates directly with the WaveLinx Wireless system for hybrid wired-plus-wireless layouts. One app. One commissioning workflow. One submittal package.
See How It Commissions Before You Spec It.
Our team will walk through the layout with you, talk through the spec, and show you exactly what commissioning looks like for your project type.