This ZIP file contains a Revit family for a Cooper Lighting : Metalux Brand fixture, as well as supporting files that are integral to the funciton of the family in a project.


Follow these steps and Extract these files to the following locations:


Step 1. Create a Windows File Folder in the Revit Library of your choice called "Cooper Lighting".

Step 2. Create a Windows File Folder within the Cooper Lighting Folder created in Step 1 called "Metalux".

Step 3. Place the un-zipped Windows product folder (e.g. "1x1-Parallux-III-P3") within the Metalux Folder created in Step 2.

	(This folder contains the necessary .TXT and .CSV Type Catalog)

Step 4. Extract any <File Name>.ies files to the IES Folder, typically installed in C:\Documents and Settings\All Users\Application Data\Autodesk\<Revit release name>